Skip to main content
DMala
Visitor II
September 10, 2018
Question

Echo Cancellation Demo is not working with Nucleo Board Setup. (Details below)

Trying to run Echo Cancellation Demo using X-NUCLEO-CCA01M1 , X-NUCLEO-CCA02M1 and NUCLEO-F446RE with FP-AUD-SMARTMIC1 Firmware, GUI. Using coupons for microphone. 

With GUI i am able to run all the demo but Echo Cancellation. 

With Echo Cancellation it seems microphone is enabled and collecting data however I do not hear anything on the speaker. Not sure what is wrong. Using 8 ohm 2 W speakers. Powered also. 

This topic has been closed for replies.