Skip to main content
DCorl.2
Visitor II
August 8, 2022
Question

Does the STEVAL-MKI109V3 have onboard support for sensor fusion using the STEVAL-MKI159V1?

..

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    August 12, 2022

    Hi @DCorl.2​ ,

    the library implementing the sensor fusion with ST sensors is the MotionFX, and it is not so straightforward to be used with STEVAL-MKI109V3, since its FW is not open-source.

    The suggestion of the UM2220 user manual is to run this implementation of the sensor fusion here:

    The software comes with sample implementation running on an X-NUCLEO-IKS01A2, X-NUCLEO-IKS01A3 or X-NUCLEOIKS02A1 expansion board on a NUCLEO-F401RE, NUCLEO-L476RG, NUCLEO-L152RE or NUCLEO-L073RZ development board.

    But of course you can configure all the device registers with the STEVAL-MKI109V3 + Unico-GUI.

    -Eleon