Skip to main content
MSant.11
Associate III
February 8, 2020
Question

Does the APWorkbench software work in STM-32 Nucleo Environment, e.g with X-NUCLEO-CCA02M2 board ?

..

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
February 11, 2020

Hi @MSant.1​ , the APWorkbench sw runs only on dedicate audio board (equipped with STA321MP), while for the NUCLEO development board you should use the Unicleo GUI. However the microphone is not supported from this GUI, so I believe that if you want to use a dedicated GUI you should use APWlink environment (plugging the STEVAL-MIC001V1 on the STEVAL-MKI126V1 board), while if you want to write a project it is better to use the Nucleo environment (FP-AUD-BVLINK1). Regards