Skip to main content
LCE
Principal III
February 21, 2024
Question

Does ST offer any IP67 microphones with analog output?

Does ST offer any IP67 microphones with analog output?

This topic has been closed for replies.

2 replies

Federica Bossi
ST Technical Moderator
February 23, 2024

Hi @LCE ,

All MEMS microphones have a hole through which water surely enters and therefore there are no water-resistant MEMS microphones on the market

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
LCE
LCEAuthor
Principal III
February 23, 2024

But as you surely have experienced, sound waves can travel through solid matter. ;)

Infineon IM73A135V01 (but that one has a differential output, I'd rather have it single-ended, but that's not specified for that mic) has at least IP57:

IP5x: Ingress of dust is not entirely prevented, but it must not enter in sufficient quantity to interfere with the safe operation of the equipment.

IPx7: Immersion, up to 1 meter (3 ft 3 in) depth Ingress of water in harmful quantity shall not be possible when the enclosure is immersed in water under defined conditions of pressure and time (up to 1 meter (3 ft 3 in) of submersion). Test duration: 30 minutes

Until recently we used a microphone from Vesper (also IP57), but that small company was bought and that product EOL'd.