Skip to main content
YGary
Associate II
November 1, 2018
Question

Does Lis3dh need do calibration at when SMT in factory to our system ?

Hi,

from Data sheet, i saw section 3.5, it says no need to further calibration

but when i check output data from register 28-2D, the value is variety time to time ,

it has variety range for +- 20 ~ +-40, is it correct? or we should do calibration at factory side?

regards

Gary

    This topic has been closed for replies.

    5 replies

    ST Employee
    November 1, 2018

    What is the unit of mentioned variance? mg? LSB?

    In any case some variance is normal, the sensor has a noise, a noise can be also induced by not completely stable environment.

    Additional calibration is not needed.

    YGary
    YGaryAuthor
    Associate II
    November 1, 2018

    Hi

    thanks for reply, i guess the unit should be mg

    output_x = (value from register 28-29) * sensitivity

    the sensitivity is define as "#define SENSITIVITY_2G 1 /** mg/LSB */"

    i also do some calculate with sqrt(output_x^2 + output_y^2 + output_z^2)

    the variance is still.

    am i go wrong with definition or something else?

    regards

    Gary

    ST Employee
    November 1, 2018

    The sensor has several modes and according to the mode the output is 8, 10 or 12 bit left adjusted in the output 16 bit register. So you have to shift right the value in output register.

    You can check your conversion is correct if you see 1g of the gravity in an axis pointing to ground.

    YGary
    YGaryAuthor
    Associate II
    November 2, 2018

    Hi,

    my setting is 10 bit with normal mode, with FS = +-2g, ODR = 100Hz

    and i've measure for 5 minutes with 5 times, the average of conversion is 1010 mg, point to ground

    regards

    Gary

    ST Employee
    November 2, 2018

    OK, it looks good.