No, SensorTile.box is just a board with LSM6DSOX on board that lets you access easily to many features, MLC included. However, there are other several platforms that support datalogging and programming of MLC, such as the combination of MKI109V3 (ProfiMEMS motherboard) and the LSM6DSOX DIL24 adapter. Moreover, if you have already collected your dataset, you can generate a decision tree and the sensor configuration file in “offline mode�? using Unico-GUI. Once the configuration file is ready, you can upload it in the sensor whenever you like.