Skip to main content
JRule
Associate
December 18, 2018
Question

Do the LIS3MDL Reserved Pins need to be connected?

Hi, we have a board with several I2C based sensors on it, including the LIS3MDL and LIS3DH.

The 3DH works like a treat, but I cant get any communication from the 3MDL. The only thing I can see that would cause this is a discrepancy with our board design and the data sheet. I was hoping someone can confirm whether the reserved pins (2 and 12) are essential for operation and need to be connected to ground to work or if its ok for them to remain Not Connected. Thanks.

This topic has been closed for replies.

6 replies

AvaTar
Senior III
December 18, 2018

Didn't the LIS3 have the combo interface, at least the LIS3MDL ?

The interface mode (I2C or SPI) is defined by an input pin. I guess you tried the "wrong" mode.

Check the schematics, and either change the hardware to get your preferred bus mode, or switch the interface.

videojames
Associate III
December 19, 2018

Hi, yes I am pulling CS mode high to enable I2C.

ST Employee
December 18, 2018

I would need to check with sensor specialist if it is mandatory to connect reserved pins to ground, personally I think it should work even if they are not connected.

Can you double check if you have correct I2C address?

Can you check the I2C signals with logic analyzer?

videojames
Associate III
December 19, 2018

Hi, I have a functioning I2C on the MSP430 which is working with TMP75 and LIS3DH. I have tried all available I2C addresses. I have used the Saelae to confirm that I get NAK when I try to communicate with the LIS3MDL.

It would be great if a sensor specialist can confirm whether or not these need to be connected. Thanks,

ST Employee
December 19, 2018

I have got the answer from sensor specialist and connections between pins 2, 12 to GND, are mandatory.