Skip to main content
IVini
Associate
February 17, 2021
Solved

Default "UCF" file for STEVAL-MKI197V1 (LSM6DSOX adapter board) when used with STEVAL-MKI109V3

  • February 17, 2021
  • 2 replies
  • 937 views

Hi,

I have configured STEVAL-MKI197V1 for Glance recognition as per ST's demo but I am not able to reset the LSM6DSOX to default so I can try other gesture recognition using ML.

I was wondering if there is a way within the Unico GUI that I can reset everything to default, thanks in advance.

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @IVini​ ,

    If you just want to reset the device (the MCL configuration together with the , but without powering off the device), you can run the SW RESET procedure descrifed in the application note AN5272 p.57.

    "If the reset to the default value of the control registers is required, it can be performed by setting the SW_RESET bit of the CTRL3_C register to 1. When this bit is set to 1, the following registers are reset to their default value:"

    • FUNC_CFG_ACCESS (01h);
    • PIN_CTRL (02h);
    • FIFO_CTRL1 (07h) through FIFO_CTRL4 (0Ah);
    • COUNTER_BDR_REG1 (0Bh) and COUNTER_BDR_REG2 (0Ch);
    • INT1_CTRL (0Dh) and INT2_CTRL (0Eh);
    • CTRL1_XL (10h) through CTRL10_C (19h);
    • FIFO_STATUS1 (3Ah) and FIFO_STATUS2 (3Bh);
    • TAP_CFG0 (56h) through MD2_CFG (5Fh);
    • I3C_BUS_AVB (62h);
    • X_OFS_USR (73h), Y_OFS_USR (74h) and Z_OFS_USR (75h).

    Basically, it should be similar to an .ucf file with all the registers set to their default value. You could export the register configuration (memory dump) before setting the MLC to keep track of your defaults.

    I also suggest you to check the available examples on Github for the different gesture recognition MLC apps.

    -Eleon

    2 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    February 17, 2021

    Hi @IVini​ ,

    If you just want to reset the device (the MCL configuration together with the , but without powering off the device), you can run the SW RESET procedure descrifed in the application note AN5272 p.57.

    "If the reset to the default value of the control registers is required, it can be performed by setting the SW_RESET bit of the CTRL3_C register to 1. When this bit is set to 1, the following registers are reset to their default value:"

    • FUNC_CFG_ACCESS (01h);
    • PIN_CTRL (02h);
    • FIFO_CTRL1 (07h) through FIFO_CTRL4 (0Ah);
    • COUNTER_BDR_REG1 (0Bh) and COUNTER_BDR_REG2 (0Ch);
    • INT1_CTRL (0Dh) and INT2_CTRL (0Eh);
    • CTRL1_XL (10h) through CTRL10_C (19h);
    • FIFO_STATUS1 (3Ah) and FIFO_STATUS2 (3Bh);
    • TAP_CFG0 (56h) through MD2_CFG (5Fh);
    • I3C_BUS_AVB (62h);
    • X_OFS_USR (73h), Y_OFS_USR (74h) and Z_OFS_USR (75h).

    Basically, it should be similar to an .ucf file with all the registers set to their default value. You could export the register configuration (memory dump) before setting the MLC to keep track of your defaults.

    I also suggest you to check the available examples on Github for the different gesture recognition MLC apps.

    -Eleon

    IVini
    IViniAuthor
    Associate
    February 18, 2021

    Thanks Eleon