Skip to main content
MKS
Associate III
July 3, 2019
Question

Data Acquisition Problem

Hi ,

i am trying to capture accelerometer data from LIS3DSH triaxial  sensor using NORDIC nrf5232 Soc.,  via i2c for a configuration of 1600 samples/sec. as it supports two slave address 1D & 1E .

when i configure for 1d and capture data is not coming  properly like 0 data or some constant data , but if i configure the same for 1e data is properly coming , only problem being 0 at some sample set. nrf52832 is set for 400 k clock , when seen in logic analyzer while capturing i am getting 200K and also in oscilloscope, i have asked the issue with Nordic as well , they say code wise everything is fine with respect to code , also without  connecting to slave clock generated is also 400K.

so help me with this issue , how to overcome.

Thank you

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    July 5, 2019

    HI @MKS​ , the I2C address selection depends on the pin 7 (SEL) value: in case the pin is at ground (0V), the I2C address will be 1E, while in the other case will be 1D (p 23 of the datasheet). How do you manage that pin on your board / with tour MCU? which Vdd / VddIO are you using, considering also the supply of the nrf5232 Soc (the recognition of a "0" or "1" logical level depends directly on Vdd)? Regards

    MKS
    MKSAuthor
    Associate III
    July 5, 2019

    hi @Eleon BORLINI​  thank you , we are connecting to vdd pin for 1D address, thank you