Skip to main content
Visitor II
Jun 12, 2026 10:42 AM UTC
Question

Create firmware target NUCLEO-L073RD+X-NUCLEO-IKS02A1 (IIS2DLPC) for AlgoBuilder (MEMS Studio)

Dear mister/misses,
 

Regarding the latest version of MEMS Studio with AlgoBuilder I have the following question:

  1. How can I create a AlgoBuilder firmware target for the NUCLEO-L073RD+X-NUCLEO-IKS02A1 (IIS2DLPC)?
  2. How to import this target in the AlgoBuilder.

The step I have taken so far:
a) Create a CubeMx file for this configuration using the MotionTL library.
b) Generate Code (open+build in CubeIDE) and program firmware in MEMS Studio using binary file obtained from CubeIDE.
c) Successfully connect to setup in MEMS studio and real-time evaluate Motion Tilt.

 

I have included the used CubeMX file for more information.

 

Kind regards,

D.