Skip to main content
NSemrHomeInit
Associate III
March 25, 2023
Question

Could not read and write the ISM330DLC each 10ms period

Dear ST Hello,

I am trying to use the ISM330DLC 3D accelerometer and gyroscope with the stm32F329Discovery board and I am facing some problems when I want to read and write all the registers every 10 ms ISR period.

I want to try to change the registers every period without compiling in changing the code each time. I am doing this to have to calibrate the filters in real time.

To do so I am defining all the registers in a header file. here is an example of the status register.

#define ISM330DLC_STATUS_REG 0x1EU
typedef volatile union
{
	uint8_t All;
	struct
	{
		uint8_t XLDA :1;	//Accelerometer new data available
		uint8_t GDA :1;	//Gyroscope new data available
		uint8_t TDA :1;	//Temperature new data available
		uint8_t Reserved :5;
	} ISM330DLC_RegBits;
} Tun_Status_Reg;

I am doing the same thing to all the registers and I am defining a union (buffer & struct) for all the ISM330DLC registers.

typedef union
{
	struct
	{
		uint8_t Reserved1; //RESERVED
		Tun_Runc_Cfg_Access FUNC_CFG_ACCESS; //FUNC_CFG_ACCESS
		uint8_t Reserved2; //RESERVED
		uint8_t Reserved3; //RESERVED	
...
	uint8_t Reserved9; //RESERVED
	} ISM330DLC_Reg_Struct;
	uint8_t ISM330DLC_Reg_Tab[ISM330DLC_MAX_BUFFER_REG];
} ISM330DLC_iDriver_Description;

I stored in an array of structures the type (RW) and the address of each register

Reg_Type_Address IMS330DLC_Reg_Type_Adr [] =
{	//adr //Type	 //R/W
	{.adr=0x00, .type=0xFF},	 //- //FF Reserved RESERVED
	{.adr=0x01, .type=0x03},	 //r/w //0x02 Read FUNC_CFG_ACCESS
	{.adr=0x02, .type=0xFF},	 //- //0x03 Write RESERVED
	{.adr=0x03, .type=0xFF}, //- RESERVED
	{.adr=0x04, .type=0x03}, //r/w ENSOR_SYNC_TIME_FRAME
	{.adr=0x05, .type=0x03}, //r/w SENSOR_SYNC_RES_RATIO
	{.adr=0x06, .type=0x03}, //r/w FIFO_CTRL1
	{.adr=0x07, .type=0x03}, //r/w FIFO_CTRL2
...
	{.adr=0x6F, .type=0x03}, //r/w INT_OIS
	{.adr=0x70, .type=0x03}, //r/w CTRL1_OIS
	{.adr=0x71, .type=0x03}, //r/w CTRL2_OIS
	{.adr=0x72, .type=0x03}, //r/w CTRL3_OIS
	{.adr=0x73, .type=0x03}, //r/w X_OFS_USR
	{.adr=0x74, .type=0x03}, //r/w Y_OFS_USR
	{.adr=0x75, .type=0x03}, //r/w Z_OFS_USR
	{.adr=0x7F, .type=0xFF}, //- RESERVED
};

I have two functions the first one is for init and the second is the task:

The init just fills up the structure with the values to be sent to the Gryro in the init phase.

the BSP_ISM330DLC_ReadWrite_Reg will be called each 10ms and read all the registers and write if any register is manually updated in the real-time watch expression.

uint16_t BSP_ISM330DLC_ReadWrite_Reg(ISM330DLC_iDriver_Description *GyroAccDriverReg, uint16_t Num)
 
{
 
	uint16_t index;
 
	uint16_t sizeofBuffer;
 
	sizeofBuffer = 40;//sizeof(GyroAccDriverReg->ISM330DLC_Reg_Tab)/sizeof(GyroAccDriverReg->ISM330DLC_Reg_Tab[0]);
 
 
 
	if(GyroAcc->ReadID() == GyroAccDriverReg->ISM330DLC_Reg_Struct.WHO_AM_I)
 
	{
 
		for (index = 0; index < sizeofBuffer ; index++)
 
		{
 
			Debugvariable.loop_counter++;
 
			if (0xFF != IMS330DLC_Reg_Type_Adr[index].type)
 
			{
 
				//check if any bit has been changed
 
				if (u8_ISM330DLC_Reg[index] != GyroAccDriverReg->ISM330DLC_Reg_Tab[index])
 
				{
 
					//bit has been changed in the driver register updated it
 
					ISM330DLC_Update_Regiter_Flag = 1;
 
				}
 
				//loop through the buffer and read write if necessary
 
				if (0x02 == IMS330DLC_Reg_Type_Adr[index].type)
 
				{
 
					//read
 
					Acc_Gyro_Ism330dlc_Read(&GyroAccDriverReg->ISM330DLC_Reg_Tab[index], IMS330DLC_Reg_Type_Adr[index].adr, Num);
 
 
 
					// Read data to a local buffer
 
					u8_TL3GD20_Reg[index] = GyroAccDriverReg->ISM330DLC_Reg_Tab[index];
 
 
 
					//reset the flag when write is done!
 
					ISM330DLC_Update_Regiter_Flag = 0;
 
				}
 
				else if (0x03 == IMS330DLC_Reg_Type_Adr[index].type)
 
				{
 
					if ((1u == ISM330DLC_Update_Regiter_Flag))
 
					{
 
						//write
 
						Acc_Gyro_Imc330dlc_Write(&GyroAccDriverReg->ISM330DLC_Reg_Tab[index], IMS330DLC_Reg_Type_Adr[index].adr, Num);
 
						//reset the flag when write is done!
 
						ISM330DLC_Update_Regiter_Flag = 0;
 
					}
 
					//read
 
					Acc_Gyro_Ism330dlc_Read(&GyroAccDriverReg->ISM330DLC_Reg_Tab[index], IMS330DLC_Reg_Type_Adr[index].adr, Num);
 
					//if write read is not good issue a problem.
 
 
 
					// Read data to a local buffer
 
					u8_ISM330DLC_Reg[index] = GyroAccDriverReg->ISM330DLC_Reg_Tab[index];
 
				}
 
				else
 
				{
 
 
 
				}
 
 
 
 
 
			}
 
		}
 
		return 1;
 
	}
 
	else
 
	{
 
		Debugvariable.id_failure++;
 
		return -1;
 
	}
 
}

My problem is when I read all the registers some of them are messy

and shifted in some cases. It looks like I read more than uint8_t somewhere and overwritten the structure. I read the datasheet all registers are 8 bits.

I pushed my code to git if you want to see the whole code.

https://github.com/semrade/Meme_project.git

This topic has been closed for replies.