Skip to main content
LWeir.775
Associate II
September 29, 2021
Question

Corrupted Data on the SD card from STWINK HS Data Logger

Reducing the number of sensors enabled in the configuration file helps, as does slowing down the SD clock (i.e. increasing hsd1.Init.ClockDiv = n in STWIN_sd.c). We've also noted that the code in sd_diskio.c has the compile time build define "ENABLE_SCRATCH_BUFFER". Please can you say if this should or should not be switched on for the StWin1b hs data logger ?

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    September 29, 2021

    Sorry, not familiar with this project.

    The scratch buffer method I originally developed for the F4 SPL addressed the unaligned memory issue when using DMA, which needs 32-bit alignment.

    It would decompose read/writes into single sector accesses via an aligned buffer, either on the stack or statically allocated.

    If you do f_read/f_write with large requests that are sector multiples, sector aligned, and with 32-bit aligned source/dest memory the scratch buffer won't be needed.

    Where things get ugly is if you do a lot of small or spanning writes which require FatFs to shuffle and deblock, using portions of your original buffer at a byte level.

    SDIO is going to be woefully inefficient with non-sector aligned file IO, you should buffer 8KB or up to 32KB and manage/wrap your output functionality to optimize writing in multiple sectors, on sector or cluster boundaries within the file.

    If you're using DMA, and randomly sized f_read/f_write, you're going to want to "double buffer" rather than "transfer in place"

    You could add an assert() to the routines in DISKIO layer to confirm this as a potential failure mechanism.

    ST's implementation for POLLED transfers is also VERY WEAK, rather than optimize the normative case, it cripples all transfers to handle the potentially unaligned ones.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..