Skip to main content
Visitor II
February 11, 2024
Question

Configuring STEVAL MK1221v1 with the black pill stm32f401ccu6

I have been trying to configure the steval mk1221v1 which is a breakout board for the lsm6dso32x imu sensor using spi 4-wire interface but can't make to work. I am not sure if i am making the right connections. I am sure I have connected the scl, sda, sdo and cs correctly but not sure what needs to be done with the vddio , sdx, scx pins. Do they need to be connected to 3.3v or left hanging. Moreover there are 2 sets of sdx and scx pins the reason for which i dont understand. Any help would be good. Thanks!

Here's the code snippet for accessing the who_am_i register.

uint8_t reg = WHO_AM_I | 0x80 ;
HAL_GPIO_WritePin(LSM_CS_GPIO_Port, LSM_CS_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, &reg, 1, HAL_MAX_DELAY);
HAL_SPI_Receive(&hspi1, &ret, sizeof(reg), HAL_MAX_DELAY);
HAL_GPIO_WritePin(LSM_CS_GPIO_Port, LSM_CS_Pin, GPIO_PIN_SET);

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
February 13, 2024

Hi @asatwik218 ,

Can you share your schematic with the actual connections? Thanks

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.