Skip to main content
Visitor II
July 13, 2024
Question

Configurations certain registers before reading whoami register contents

Hello,

I'm currently working with the ICM-20602 IMU sensor and the LSM6DSV16X IMU sensor in an STM32-based project using STM32CubeIDE for stm32f446re. I've successfully interfaced with the ICM-20602 sensor and am able to read the WHO_AM_I register after ensuring that the sensor is out of sleep mode by configuring the POWER MANAGEMENT 1 register.

 

Here is the relevant code I used for the ICM-20602 sensor:

 

/* Function to read a register from the ICM-20602 via SPI */

uint8_t spi_read_register(uint8_t reg_addr) {

uint8_t tx_buf[2] = { reg_addr | 0x80, 0 }; // MSB set for read operation

uint8_t rx_buf[2] = { 0, 0 };

 

HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_RESET); // Set CS low

HAL_SPI_TransmitReceive(&hspi3, tx_buf, rx_buf, 2, HAL_MAX_DELAY);

HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_SET); // Set CS high

return rx_buf[1];

}

 

/* Function to write to a register over SPI */

void spi_write_register(uint8_t reg_addr, uint8_t value) {

uint8_t tx_buf[2] = { reg_addr & 0x7F, value }; // MSB cleared for write operation

HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_RESET); // Set CS low

HAL_SPI_Transmit(&hspi3, tx_buf, 2, HAL_MAX_DELAY);

HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_SET); // Set CS high

}

 

/* Function to enable necessary bits in POWER MANAGEMENT 1 register */

void enable_power_management(void) {

uint8_t pm1_data = spi_read_register(PWR_MGMT_1_REG_ADDR);

pm1_data &= ~SLEEP_BIT; // Clear SLEEP_BIT to exit sleep mode

spi_write_register(PWR_MGMT_1_REG_ADDR, pm1_data);

}

 

/* Function to read the WHO_AM_I register */

void read_who_am_i(void) {

uint8_t who_am_i = spi_read_register(WHO_AM_I_REG_ADDR);

char buffer[50];

sprintf(buffer, "WHO_AM_I register: 0x%02X\r\n", who_am_i);

UART_Transmit(buffer);

}

For the ICM-20602 sensor, I needed to clear the sleep bit (bit 6) in the POWER MANAGEMENT 1 register (address 0x6B) to ensure the sensor is active. After this configuration, reading the WHO_AM_I register returns the correct value of 0x12.

 

Now, I am working with the LSM6DSV16X sensor. When I try to read the WHO_AM_I register, I receive an incorrect value (0x80 instead of the expected 0x70). 

 

My question is: Do I need to configure any specific registers or perform any initialization steps for the LSM6DSV16X sensor before reading the WHO_AM_I register, similar to the power management configuration required for the ICM-20602 sensor?

 

 

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
July 22, 2024

Hi @Apuroop ,

No, it is not necessary for LSM6DSV16X.

I suggest you to follow our official examples on Github to implement the WhoAmI reading.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.