Skip to main content
Associate
January 22, 2025
Solved

Compatibility of the IMP23ABSUTR Sensor with Vapor Phase Reflow Ovens

  • January 22, 2025
  • 6 replies
  • 939 views

Hello,

Can the IMP23ABSUTR sensor go through a vapor phase oven?"

Thx.

 

 

Best answer by Federica Bossi

Hi @Moe_Rice ,

it is not recommended to solder microphones with that technique, because they have a hole through which contamination enters. I suggest you use IR reflow ovens.

6 replies

Andrew Neil
Super User
January 22, 2025

Did you look at the "Soldering Information" section in the datasheet?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Moe_RiceAuthor
Associate
January 22, 2025

Hello,

The datasheet does not specifically mention vapor phase soldering. It generally refers to the compatibility of the IMP23ABSUTR sensor with the reflow soldering process and provides a recommended thermal profile for lead-free (Pb-free) soldering.

The term "vapor phase" is not explicitly mentioned in the documentation, and the information provided mainly concerns temperature parameters, preheat time, duration above the melting temperature, and peak temperature. In my opinion, these guidelines could potentially be adapted to different types of reflow processes, including vapor phase soldering, but this would require specific validation.

Thx

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
January 29, 2025

Hi @Moe_Rice ,

it is not recommended to solder microphones with that technique, because they have a hole through which contamination enters. I suggest you use IR reflow ovens.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Andrew Neil
Super User
January 29, 2025

Sounds like that should be explicitly explained in the datasheet?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Visitor II
December 19, 2025

I have notice IMP23ABSUTR NRND.  

Did thst mens it will be face out.  If yes.  Is there any replacement  upcomming for 80khz ultrasonic  mems microphone?