Skip to main content
sw lee
Associate
April 24, 2018
Question

Cann't complie to eMotionV2_REL_5.0.0.zip(in en.stsw-mki109w.zip)?

Posted on April 24, 2018 at 10:20

Hi..

i use steval-mki1092V2(demo board) with mki160V1(sensor)..

so i was download to en.stsw-mki109w.zip(for Windows) file...

and  i use to IAR Embeded Work...7.20 Version...

so when i open project file,

come to msg like this.. 

'Broken Options were detected in the project file A backup copy will be made'

(See log window for detail)'

and next msg is...

--> The project 'emotion' contains the unknown to 'CADI_ID'

-->

The project 'emotion' contains the unknown to 'TIFET_ID'

is it need upgrade to IAR 7.70 version ??

thanks..

mailto:xfile2580@daum.net

    This topic has been closed for replies.