Skip to main content
JPale
Associate II
November 16, 2019
Question

Can we put con-formal coating and epoxy on APluseG (LSM6DSM)sensor?

will con-formal & epoxy coating effect the functionality of sensor ?

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    November 18, 2019

    Hi @JPale​ , in general yes, you can put con-formal coating on ST inertial sensors. No worry about the temperature of deposition for an epoxy if below 125°C (consider that the temperature peak during the solder phase is much higher). However, you should keep care of the residual mechanical stress on the package. You have to try to depose uniformly the epoxy resin under a not too high temperature. To avoid possible inaccuracies, if possible for you should test the device before the coating deposition, then after this treatment and check the residual offset: you will compensate it using the registers 73h, 74h, 75h of LSM6DSM. Regards

    JPale
    JPaleAuthor
    Associate II
    November 19, 2019

    Thank You Eleon BROLINI.