Skip to main content
Eleon BORLINI
ST Employee
December 1, 2021
Solved

Can we fine tune the activity recognition example for MLC available on GitHub?

..

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    December 1, 2021

    Absolutely yes, ST offers on GitHub not only the configuration files which can be used to program the sensor for a quick start, but also configuration details (in the README file), and examples of dataset which can be used to generate the final configuration. The configuration can be fine-tuned using new datasets or different MLC parameters.

    1 reply

    Eleon BORLINI
    Eleon BORLINIAuthorBest answer
    ST Employee
    December 1, 2021

    Absolutely yes, ST offers on GitHub not only the configuration files which can be used to program the sensor for a quick start, but also configuration details (in the README file), and examples of dataset which can be used to generate the final configuration. The configuration can be fine-tuned using new datasets or different MLC parameters.