Skip to main content
JTam.1
Associate III
May 6, 2021 12:33 AM UTC
Solved

Can the time domain output of FFT calculation from MotionSP be speed (mm/s RMS), not acceleration on Y-axis?

Hi, Can the time domain output of FFT calculation from MotionSP be speed (mm/s RMS), not acceleration on Y-axis? Please advise. Thanks!

    This topic has been closed for replies.
    niccolò
    niccolòBest answer
    ST Employee
    May 6, 2021 7:27 AM UTC

    Hi @JTam.1​ ,

    in the sTimeDomainData_t structure variables you have the speed variable in the time domain data, but it is derived from the FFT circular buffer.

    if you try to use that to compute the FFT you will have a delayed output withan error due to approximation and calculation error and noise error propagation.

    the best way should be to develop an integration algorithm and then compute the FFT with another library, but even in this case, it is not advised to use the acceleration integration as the core of your computation.

    hope this helps

    Niccolò

    1 reply

    niccolò
    niccolòBest answer
    ST Employee
    May 6, 2021 7:27 AM UTC

    Hi @JTam.1​ ,

    in the sTimeDomainData_t structure variables you have the speed variable in the time domain data, but it is derived from the FFT circular buffer.

    if you try to use that to compute the FFT you will have a delayed output withan error due to approximation and calculation error and noise error propagation.

    the best way should be to develop an integration algorithm and then compute the FFT with another library, but even in this case, it is not advised to use the acceleration integration as the core of your computation.

    hope this helps

    Niccolò