Skip to main content
Associate II
September 10, 2024
Solved

Can the LPS27HHW be used to detect non-water liquids, such as oil?

Hi Sir,

 

Can the LPS27HHW be used to detect non-water liquids, such as oil?

 

 

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
September 19, 2024

Hi @TIENHUA ,

Theoretically it is possible to see other liquid respect to water. The only issue is due to chemical material is present into the liquid you are referring. This can cause a damage of the gel present in the device. In case of some particles passes the gel, the device doesn't work properly. The suggestion is to test the device in desired liquid.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
September 19, 2024

Hi @TIENHUA ,

Theoretically it is possible to see other liquid respect to water. The only issue is due to chemical material is present into the liquid you are referring. This can cause a damage of the gel present in the device. In case of some particles passes the gel, the device doesn't work properly. The suggestion is to test the device in desired liquid.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.