Skip to main content
Associate
May 19, 2026
Solved

Can the embedded state machines in the LSM6DS032 be programmed over I2C?

Hello, I am looking to use the LSM6DS032 accelerometer + gyroscope in a project, I intend to interface it with an MCU via I2C. I am wondering if it is possible to program the embedded finite state machines in the accelerometer using only I2C and writing to registers, and if there are any guides or application notes on how this can be done?

Chris21
Chris21Best answer
Associate II
May 19, 2026

There is documentation: https://www.st.com/en/mems-and-sensors/lsm6dso32.html#documentation

Datasheet says, "The registers embedded inside the LSM6DSO32 may be accessed through both the I²C and SPI serial interfaces."

And there is AN5505...

https://www.st.com/resource/en/application_note/an5505-lsm6dso32-finite-state-machine-stmicroelectronics.pdf 

.

2 replies

Chris21
Chris21Best answer
Associate II
May 19, 2026

There is documentation: https://www.st.com/en/mems-and-sensors/lsm6dso32.html#documentation

Datasheet says, "The registers embedded inside the LSM6DSO32 may be accessed through both the I²C and SPI serial interfaces."

And there is AN5505...

https://www.st.com/resource/en/application_note/an5505-lsm6dso32-finite-state-machine-stmicroelectronics.pdf 

.
Associate III
May 19, 2026

https://www.st.com/resource/en/design_tip/dt0064-noise-analysis-and-identification-in-mems-sensors-allan-time-hadamard-overlapping-modified-total-variance-stmicroelectronics.pdf

Page 3 there appears to be a math errror in the MATLAB code,

Ts = 1/FS not Ts = 1/Ts, the units do not match.  

PS The thermal noise in the acceleration signals are important for Structural Health Monitoring.