Skip to main content
LeiNie
Visitor II
February 6, 2019
Question

Can someone with internal knowledge confirm that the LIS3DSH in I2C mode never drives the SCL line low and that a standard "single master push-pull SCL" can be used in combination with the bidirectional SDA line.

The LIS3DSH datasheet contains the following text (not very clear):

"If a receiver can’t receive another complete byte of data until it has performed some other function, it can hold the clock line, SCL LOW, to force the transmitter into a wait state. Data transfer only continues when the receiver is ready for another byte and releases the data line"

I guess it should have been "the clock line" - anyway I have implemented the I2C bus as a single master SCL-push-pull / SDA-bidirectional - and it works flawlessly at 100KHz - but before releasing this for final PCB design I would like a confirmation of my SCL-push-pull approach.

- thanks in advance.

Best regards

Leif

This topic has been closed for replies.