Skip to main content
DTali
Associate II
January 9, 2020
Question

Can i use LSM6DSO MEMS with 6KHz odr with i2c bus?

I see that i2c operate up to 400Hz

This topic has been closed for replies.

4 replies

Ozone
Principal
January 9, 2020

You might want to check if a read-multiple-bytes scenario provides enough bandwidth.

Just add up the number of transfer cycles required, and compare it to the time frame of a 6kHz update rate.

In SPI mode, the LSM6D allows up to 10MHz.

DTali
DTaliAuthor
Associate II
January 9, 2020

With SPI everything is ok. Question is can i reach same ODR with i2c?

Ozone
Principal
January 9, 2020

> Question is can i reach same ODR with i2c?

So check it by doing said calculation, or an appropriat software implementation.

Such bandwidth calculations are the SW engineering standard tasks.

DTali
DTaliAuthor
Associate II
January 9, 2020

it looks that everything is ok. i will also try fifo mode to increase productivity.