Skip to main content
sam239955
Associate III
September 29, 2011
Question

Button with GPIO and Blueooth possible?

Posted on September 29, 2011 at 13:23

Hi,

my question is if it's possible to connect a button to the inemo v2 board which I need in an application as start button (or can i use one of the buttons on board, but how can I get the button status (pressed = true/false) with the DLL?

other question is that I have a bluetooth module that uses i2c, can I connect it with the iNemo via the pin connectors? Is that possible?

regards

Alex
    This topic has been closed for replies.