Skip to main content
AvaTar
Senior III
May 2, 2015
Question

bug in STSW-MKI109L SW package installer ?

Posted on May 02, 2015 at 20:28

Seems there is a bug in the Linux installer for the MKI109V2 software package.

Calling the 'unico' executable failed persistently with ''

no permission

'' error, even as root.

Setting the '

x

' flag for unico (

chmod

command) fixed the issue - the installer just omitted to make the executable 'executable'.

System was a i386 Linux Mint 17 XFCE, which, as a Ubuntu derivative, is assumed to fall in the ''Debain-like OS'' class.

#stsw-mki109l-unico-installer-bug
This topic has been closed for replies.