Skip to main content
Associate II
April 18, 2024
Solved

Bug in LSM6DSV16X driver v3.0.0, COUNTER_BDR_REG1/COUNTER_BDR_REG2 configured wrong

Hello,

I just wanted to inform you that there is a bug in the ST driver for the LSM6DSV16X v3.0.0, available on Github.

Function lsm6dsv16x_fifo_batch_counter_threshold_set is wrongly setting the 2 register values, and for COUNTER_BDR_REG1 it is not ensuring that other bit fields are not changed.

I stumbled upon this after some time trying to get the BDR counter threshold interrupt to work in a prototype, and thought to share it here.

I changed that function implementation to the code below (basically a copy from the LSM6DSOX driver), and it works fine now:

int32_t lsm6dsv16x_fifo_batch_counter_threshold_set(const stmdev_ctx_t *ctx,
 uint16_t val)
{
 lsm6dsv16x_counter_bdr_reg1_t counter_bdr_reg1;
 lsm6dsv16x_counter_bdr_reg2_t counter_bdr_reg2;
 int32_t ret;

 ret = lsm6dsv16x_read_reg(ctx, LSM6DSV16X_COUNTER_BDR_REG1,
 (uint8_t *)&counter_bdr_reg1, 1);

 if (ret == 0)
 {
 counter_bdr_reg2.cnt_bdr_th = 0x00FFU & (uint8_t)val;
 counter_bdr_reg1.cnt_bdr_th = (uint8_t)(0x0700U & val) >> 8;
 ret = lsm6dsv16x_write_reg(ctx, LSM6DSV16X_COUNTER_BDR_REG1,
 (uint8_t *)&counter_bdr_reg1, 1);
 }

 if (ret == 0)
 {
 ret = lsm6dsv16x_write_reg(ctx, LSM6DSV16X_COUNTER_BDR_REG2,
 (uint8_t *)&counter_bdr_reg2, 1);
 }

 return ret;
}

Regards,

Rafael

 

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
May 2, 2024

Hi @rafael_daciuk ,

Can you try this new release and let me know if you solve?

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

Federica Bossi
ST Technical Moderator
May 2, 2024

Hi @rafael_daciuk ,

Thank you for pointing that out, you are right. The team is working on fixing the bug as soon as possible, I will let you know as soon as we release a new version with the fix.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
May 2, 2024

Hi Federica,

Glad to know you are already working on a fix.

I'm looking forward to getting the updated driver code.

Thank you,

Rafael

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
May 2, 2024

Hi @rafael_daciuk ,

Can you try this new release and let me know if you solve?

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
May 7, 2024

Hi @Federica Bossi,

This new version of the driver worked for me.

Thank you for the update.

Regards,

Rafael