Skip to main content
darla14
Associate III
March 30, 2019
Question

Bluetooth PIN (not GPIO) to connect with the STEVAL-BCNKT01V1 (Bluecoin) Board from WIndows 10 PC.

What will be the PIN to connect to the Bluecoin board via bluetooth from the Windows 10 PC. I see a message "Enter the pin for AM1V340?

Is it possible to connect via Windows 10?Can you please share the procedure/document stating the method.

Many thanks !

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    April 1, 2019

    hi, for my understanding which is your target purpose? Do you want to interface the Bluecoin with your PC (with win10) via Bluetooth? If so, which FW is running on the Bluecoin MCU?

    Btw, if you have to enter a PIN you can try a standard as 000000 or 123456. However, after enabling the BLE communication between your PC and the Blucecoin, you have to build up an interface acting ad BLE receiver on your PC, if you want to use the BLE trasmission.

    You can check this link for an SDK running on Linux for the host PC-Bluceoin interface management

    https://github.com/STMicroelectronics/BlueSTSDK_Python

    Btw, if you want to test and log the sensors, I suggest you to use the Unicleo environment (X-NUCLEO-IKS01A2 + Unicleo-GUI)

    Regards

    darla14
    darla14Author
    Associate III
    April 1, 2019

    Thanks 123456 worked !.(Not 000000) and also the Sensor Logging using the FP-SENS-ALLMEMS1 + Unicleo-GUI