In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
The audio signal is obtained from the digital MEMSM Kefeng as a 1-bit PDM signal, which is then converted into a 16 bit PCM sample by a PDM to PCM conversion filter at 16 kHz. Using the AcousticBF algorithm in FP-AUD-SMARTMIC1, can a sampling rate of 48KHZ be achieved
Unfortunately this is not possible: the library only works up to 16KHz, both input and output. We don't have libraries or examples that from a 16KHz input signal would allow a 48KHz output signal.
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.