Skip to main content
Visitor II
Jul 28, 2025 5:06 AM UTC
Solved

Best Wireless Data Collection Method for STEVAL-MKI109 + MEMS Sensors?

Hi everyone,

I'm starting a project using the STEVAL-MKI109D motherboard with the following sensor adapter boards:

  • STEVAL-MKI247A 

  • STEVAL-MKI240KA 

My main goal is to collect sensor data wirelessly for analysis, rather than being tethered to a PC with a USB cable. I'm trying to figure out the best approach and would appreciate some advice on the options I've considered.

This topic has been closed for replies.
bosco.stefano
bosco.stefanoBest answer
ST Employee
Aug 1, 2025 6:26 AM UTC

Hi Ardalan,
the purpose of STEVAL-MKI109D is to evaluate the device soldered on DIL24 and the source code is closed.
The best solution to use STEVAL-MKI240KA and STEVAL-MKI247A in "wireless" mode using Bluetooth or SD card (avoiding USB cable and PC), is to select STEVAL-MKBOXPRO as main board.
In this board all requested features are present (see following link: https://www.st.com/en/evaluation-tools/steval-mkboxpro.html)

Best regards.

1 reply

bosco.stefano
bosco.stefanoBest answer
ST Employee
Aug 1, 2025 6:26 AM UTC

Hi Ardalan,
the purpose of STEVAL-MKI109D is to evaluate the device soldered on DIL24 and the source code is closed.
The best solution to use STEVAL-MKI240KA and STEVAL-MKI247A in "wireless" mode using Bluetooth or SD card (avoiding USB cable and PC), is to select STEVAL-MKBOXPRO as main board.
In this board all requested features are present (see following link: https://www.st.com/en/evaluation-tools/steval-mkboxpro.html)

Best regards.