Skip to main content
cbrower
Visitor II
December 13, 2013
Question

Behavior of LIS3DH past range limits

Posted on December 13, 2013 at 19:45

If the LIS3DH range is set to +/- 2g, how does the chip behave if acceleration exceeds 2g's? Do the axis outputs limit, wrap around, go to some fixed value, etc?

This topic has been closed for replies.

1 reply

Thiago REIS
Associate II
January 10, 2014
Posted on January 10, 2014 at 14:21

Hello Charles,

the output value will show the maximum value allowed by that full scale.

In this case, for 2g, if you apply a 4g acceleration, the output will show the maximum of 2g.

Thank you,

Thiago Reis