Question
Audio Scene Classification- FP-AI-SENSING1- WITH 6 NO. OF AUDIO FILES
Hi,
I am trying to test the ASC with 6 classes and 6 audio files. Am modifying the same python script from the function pack and trying to create the Tensorflowlite model. Is that possible to add more classes or only we can use 3 classes?
If we can use maximum 3 classes, but am trying to convert 6 Audio files into model file, then what would be the option to procedure?
Thanks & Regards,
Shivashankari