Skip to main content
Associate II
Nov 8, 2025 3:58 PM UTC
Question

asm330lhhxg1 works at VDD/VDDIO=1.8V but does not work if VDD/VDDIO set to 3.3V

..

1 reply

Federica Bossi
ST Technical Moderator
Dec 24, 2025 9:41 AM UTC

Hi @arifkhan ,

If the ASM330LHHXG1 sensor works correctly at 1.8 V for VDD/VDDIO but fails at 3.3 V, possible causes include:

  • Power supply stability: Check for noise or voltage dips at 3.3 V that might affect the sensor.
  • IO level mismatch: Ensure your MCU or interface logic levels are compatible with the sensor’s VDDIO voltage.
  • Incorrect wiring or configuration: Double-check power pins and decoupling capacitors for the 3.3 V setup.
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.