Skip to main content
Associate
October 23, 2023
Solved

asm330lhhx scale factor for each x, y, z axis

  • October 23, 2023
  • 1 reply
  • 988 views

Hello,

For the asm330lhhx device, when does the scale value change and get set?  I am trying to determine if the scale factor needs to be checked only once at power up or continually while reading the raw x, y, and z values for both the gyro and the accelerometer.

In Linux Terminal, the scale and raw values show up as the following for the x component of the gyro: 

in_anglvel_x_scale

in_anglvel_x_raw

 

I plan to read the scale once and the raw value continuously.  But if the scale value changes, then I need to read both continuously.  Please confirm how they work as the datasheet was not clear on this.

Thank you!

This topic has been closed for replies.
Best answer by BPEngineer

I see now that you can set the scale value yourself.  Please close this issue.

1 reply

BPEngineerAuthorBest answer
Associate
October 23, 2023

I see now that you can set the scale value yourself.  Please close this issue.