Skip to main content
Associate III
Aug 22, 2025 8:40 AM UTC
Solved

ASM330LHH CTRL9_XL DEVICE_CONF

It is recommended that CTRL9_XL DEVICE_CONF in ASM330LHH always set this bit to 1 when configuring the device, but when should it be set back to 0? Should it not be set back?

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Aug 28, 2025 1:31 PM UTC

Hi @ggob ,

Once the device configuration is completed and stable, this bit can be set back to 0 if no further configuration changes are expected.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Aug 28, 2025 1:31 PM UTC

Hi @ggob ,

Once the device configuration is completed and stable, this bit can be set back to 0 if no further configuration changes are expected.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ggobAuthor
Associate III
Aug 28, 2025 11:54 PM UTC

Thank you very much. This is very helpful.
Is it necessary to set this bit to “1” before setting it to “1” by operating BOOT or SW_RESET of CTRL3_C?