Skip to main content
Visitor II
Nov 3, 2024 7:57 AM UTC
Question

ASM330LHB performance?

Hello,

ASM330LHB 6-axis sensor, can it reach 0.001g?

ASM330LHB 6-axis sensor that can reach 0.001g? how high can it reach?

Which 6-axis sensor is more accurate?

Can they both output angles?

 

This post has been translated from Chinese to comply with the ST Community guidelines.

 
 
This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
Nov 8, 2024 1:54 PM UTC

Hi @1232 ,

The maximum value that the sensor can reach and also the accuracy depend on the full scale you set according to datasheet:

FedericaBossi_0-1731073939188.png

If you want to reach higher g you can look at LSM6DSV32X that has a maximum full scale of 32g, but not that it is not for ASIL B automotive applications.

Can they both output angles? Yes.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.