Skip to main content
AHolt.1
Visitor II
December 13, 2019
Question

Are there any application notes on using H3LI5331DLT for shock detection? Peak shock detection?

..

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    December 16, 2019

    HI @AHolt.1​ , the H3LIS331DL has an embedded "peak" detection feature that enables you to detect a signal that exceeds a certain thresholds and lasts at least 2 ODR or more. Supposing to set a proper full-scale (e.g. 400g), you can detect a shock tuning the height of the shock with the INT1_THS (32h) register and its duration INT1_DURATION (33h). Directly reporting from Wikipedia, both of these parameters are equally important for the shock detection:

    The form of the shock pulse and particularly the duration are equally important. For example, a short 1 ms 300 g shock has little damage potential and is not usually of interest but a 20 ms 300 g shock might be critical.

    Btw, which kind of shock do you want to detect?

    Regards