Skip to main content
aaron
Associate II
Mar 12, 2014 11:22 PM UTC
Question

Application note for LPS25H?

Posted on March 13, 2014 at 00:22

I am interested in the LPS25H MEMS barometer chip, but I am having a hard time figuring out the footprint of the HCLGA-10L package.

Here is what is called out in the datasheet:

0690X00000605TMQAY.png

I cannot decipher from his what the dimensions of the pads should be.  I believe that e1/2 might give me the width, but I cannot determine the length.  Maybe that's what B is supposed to mean, but I don't see it.

Also, I found that there is a

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00064026.pdf

but cannot find one for the LPS25H.  I realize it's a very new part, but this would help -- it provides some guidance on how the pads should be laid out.

Can someone more mechanically inclined parse this for me?

Thanks.

#hclga-10l
This topic has been closed for replies.

4 replies

aaron
aaronAuthor
Associate II
Mar 15, 2014 1:28 PM UTC
Posted on March 15, 2014 at 14:28

For reference, here is the figure of merit from the LPS331AP, which is a comparable part (though with worse resolution).

0690X00000605TRQAY.png

T1 and T2 give the dimensions of the pads, and the rest can be inferred easily.

I suppose I should just use the LPS331AP instead...

gh_it
Associate
Aug 8, 2014 9:33 AM UTC
Posted on August 08, 2014 at 11:33

Getting support for ST is much harder than getting blood out of a stone.  They are at Rev 3 of this data sheet and still haven't dealt with this problem.

Freescale make a couple of nice parts which are similar in price.

Nickname3460_O
Visitor II
Oct 2, 2014 5:10 AM UTC
Posted on October 02, 2014 at 07:10

Hello,

Infact we are going to improve the quality of the drawing with more details;

The pad dimension you are looking for are: 0.30mm x 0.45mm (+/- 0.05 mm tolerance)

You can find the LPS25H AN just below the LPS331AP , at this address

http://www.st.com/stonline/stappl/resourceSelector/app?page=fullResourceSelector&doctype=application_note&SubClassID=1316

Thank you for your questions

Visitor II
Dec 23, 2024 9:27 AM UTC

Please update the entire datasheet while you're at it. The "Application hints" page is very hard to read like this, a footprint is not a schematic... And Table 2 could use an update as well like input/output/open collector info etc. And I'd expect some information on how long a measurement takes, min/typ/max etc.