Skip to main content
Visitor II
October 2, 2024
Question

Anti-alias IIS2DLPC

I am trying to configure the IIS2DLPC for anti-aliasing as indicated by figure 3 section 3.4 of an5201.

AquaKnott_0-1727894408202.png

I am seeing frequency folding in the spectrum. I am playing a 300 and 500 Hz sine wave alternately on a sound table to vibrate the sensor. Each tone plays for 1.5s then switches frequency.

AquaKnott_2-1727896501799.png

I had the IIS2DLPC configured for, High Performance, 1600Hz ODR, and Band Width ORD/4 or 400Hz. I was expecting the 500Hz to be strongly attenuated. Is my understanding of how the anti-aliasing filter works, or my setup incorrect?

Here is the config code

 

 status = iis2dlpc_power_mode_set(&iis2dlpcctx, iis2dlpc_mode_t::IIS2DLPC_HIGH_PERFORMANCE); //IIS2DLPC_HIGH_PERFORMANCE_LOW_NOISE);
 report(status);

 status = iis2dlpc_data_rate_set(&iis2dlpcctx, iis2dlpc_odr_t::IIS2DLPC_XL_ODR_1k6Hz);//iis2dlpc_odr_t::IIS2DLPC_XL_ODR_12Hz5);//iis2dlpc_odr_t::IIS2DLPC_XL_ODR_1k6Hz);
 report(status);

 status = iis2dlpc_filter_bandwidth_set(&iis2dlpcctx, iis2dlpc_bw_filt_t::IIS2DLPC_ODR_DIV_4);
 report(status);

 // Set scale 2g/4g/8g/16g
 status = iis2dlpc_full_scale_set(&iis2dlpcctx, iis2dlpc_fs_t::IIS2DLPC_8g);
 report(status);

 

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
November 8, 2024

Hi @AquaKnott ,

what is the amplitude of the input signal? and what are the units of measurement of your plot?

 

Thanks

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.