Skip to main content
PDand.1
Associate
September 3, 2020
Question

Alternative IMU for ISM330DHCX, but with CAN interface...

Hi,

I am developing an autonomously navigating robot that uses IMU for Localization and Mapping... a typical ML/Self-driving car application. I was looking for IMUs having accelerometer with +-2g sensitivity. The [INEMO-M1](http://www.digikey.in/product-detail/en/stmicroelectronics/INEMO-M1/497-14191-ND/4542053?_ga=2.141927986.1620169342.1599042795-1084286621.1599042795) was great as its packaging was easy to interface with our processing unit: the NViDIA Jetson Xavier AGX.

But it seems that it is obsolete now. I would like alternatives to it. On looking at inertial modules like ISM330DHCX, that can be interfaced with the Xavier uing CAN interface ...

Thanks and Regards,

Prashant

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
September 3, 2020

Hi @PDand.1​ , while waiting for more eventual support from community users, please check this other thread on similar topic. Regards