Skip to main content
Associate
June 4, 2024
Solved

AIS2IH Read Data Registers

Hi,

I am using AIS2IH.

I  can see in terminal   window of my computer

that registers of  data and temperature are zero's.   0 0 0  ...

My program use the setup:

 

ais2ih_cs_mode_set(&dev_ctx, AIS2IH_PULL_UP_DISCONNECT);
ais2ih_i2c_interface_set(&dev_ctx, AIS2IH_I2C_DISABLE);
ais2ih_spi_mode_set(&dev_ctx, AIS2IH_SPI_4_WIRE);
ais2ih_reset_set(&dev_ctx, PROPERTY_ENABLE);

platform_delay(0x00333333);
ais2ih_reset_get(&dev_ctx, &rst);

platform_delay(0x00333333);
ais2ih_reset_get(&dev_ctx, &rst);

platform_delay(0x00333333);
ais2ih_cs_mode_set(&dev_ctx, AIS2IH_PULL_UP_DISCONNECT);
ais2ih_i2c_interface_set(&dev_ctx, AIS2IH_I2C_DISABLE);
ais2ih_spi_mode_set(&dev_ctx, AIS2IH_SPI_4_WIRE);
/* Set full scale */
ais2ih_full_scale_set(&dev_ctx, AIS2IH_2g);
/* Set Output Data Rate */
ais2ih_data_rate_set(&dev_ctx, AIS2IH_XL_ODR_400Hz);
ais2ih_filter_path_set(&dev_ctx, AIS2IH_LPF_ON_OUT);
ais2ih_filter_bandwidth_set(&dev_ctx, AIS2IH_ODR_DIV_4);
ais2ih_self_test_set(&dev_ctx, AIS2IH_XL_ST_DISABLE );
/* Configure power mode */
ais2ih_power_mode_set(&dev_ctx, AIS2IH_HIGH_PERFORMANCE_LOW_NOISE);

memset(data_raw_acceleration, 0x00, 3 * sizeof(int16_t));
ais2ih_acceleration_raw_get(&dev_ctx, &data_raw_acceleration);

ais2ih_temperature_raw_get(&dev_ctx, &data_raw_temperature);

ais2ih_status_dup_get(&dev_ctx,& reg3);

sprintf((char *)tx_bufferL,"\n\t\r A[r]:%d,%d,%d; T[C]:%d; R:%u,DUP=%u",data_raw_acceleration[0],data_raw_acceleration[1],data_raw_acceleration[2],data_raw_temperature,tempraw,reg3);
strcat(tx_buffer, tx_bufferL);

strcat(tx_buffer,"\r\n\0");
tx_com(tx_buffer, strlen((char const *)tx_buffer));

 

 

 

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
June 5, 2024

Hi @scboris ,

Can you share a photo of your setup?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

13 replies

scborisAuthor
Associate
June 4, 2024

Whats wrong with my accelerometer?

Thank You

scborisAuthor
Associate
June 4, 2024

The  result is:

A[r]:0,0,0; T[C]:0; R:4,DUP=0

 

There R:4 is the AIS2IH_CTRL2 register value

scborisAuthor
Associate
June 4, 2024

What changes I  can made to get  the real values of the acceleration  or  temperature.

Thank You

Federica Bossi
ST Technical Moderator
June 4, 2024

Hi @scboris ,

Welcome to ST Community!

Can you try to implement our official example on github and let me know if you still have the problem?

Thanks.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
scborisAuthor
Associate
June 4, 2024

OK!

scborisAuthor
Associate
June 4, 2024

Thank You!

I changed the code of the program as it is in the link above. I take the

ais2ih_read_data_polling.c

example.

  I take another AIS2Ih accelerometer. 

But still, It is  no changes at   the result.

 

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
June 5, 2024

Hi @scboris ,

Can you share a photo of your setup?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
scborisAuthor
Associate
June 5, 2024

Hi Federica!

What is the  setup?

Hardware(schematic diagram?) or software() or timing diagram of the setup?

void ais2ih_init(void)
{
/* Initialize mems driver interface. */
stmdev_ctx_t dev_ctx;
ais2ih_reg_t int_route;
dev_ctx.write_reg = platform_write;
dev_ctx.read_reg = platform_read;
dev_ctx.handle = &SENSOR_BUS;
/* Initialize platform specific hardware */
platform_init();
/* Wait sensor boot time */
platform_delay(BOOT_TIME);
ais2ih_reset_set(&dev_ctx, PROPERTY_ENABLE);
platform_delay(0x08333333);
ais2ih_reset_get(&dev_ctx, &rst);
platform_delay(0x08333333);
platform_delay(0x08333333);
ais2ih_reset_get(&dev_ctx, &rst);
platform_delay(0x08333333);
ais2ih_cs_mode_set(&dev_ctx, AIS2IH_PULL_UP_DISCONNECT);
platform_delay(0x08333333);
ais2ih_i2c_interface_set(&dev_ctx, AIS2IH_I2C_DISABLE);
platform_delay(0x08333333);
ais2ih_spi_mode_set(&dev_ctx, AIS2IH_SPI_4_WIRE);
platform_delay(0x08333333);

}

scborisAuthor
Associate
June 6, 2024

So, the problem is with setup of the sensor.

Federica Bossi
ST Technical Moderator
June 6, 2024

Can I see your hardware?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
scborisAuthor
Associate
June 6, 2024

OK?