Skip to main content
Sijun Kim
Visitor II
May 23, 2018 6:18 AM UTC
Solved

Advantages of using integrated sensors like LSM9DS1

Posted on May 23, 2018 at 08:18

Hello, I'm going to develop a kind of solutions for local positioning, and wondering the benefits of using integrated sensors (accelerometer, gyro, and magnetometer) like LSM9DS1 over using individual sensors and gathering.

As I can handle each sensor like LSM6DSL and LIS2MDL, I think I can make data like from LSM9DS1.

Are the data from LSM9DS1 sensor better in terms of accuracy, speed, or any other things?

Thank you for your answer in advance!

#mems #lsm9ds1
This topic has been closed for replies.
Miroslav BATEKBest answer
ST Employee
May 23, 2018 2:37 PM UTC
Posted on May 23, 2018 at 16:37

The only benefit which I see is that all is in one package, so the occupied area on PCB is smaller.

But the LSM9DS1 is quite old device, the combination of LSM6DSL + LIS2MDL is much better option.

In terms of accuracy, current consumption, embedded features, and so on the combination of these two devices is much better.

1 reply

Miroslav BATEKBest answer
ST Employee
May 23, 2018 2:37 PM UTC
Posted on May 23, 2018 at 16:37

The only benefit which I see is that all is in one package, so the occupied area on PCB is smaller.

But the LSM9DS1 is quite old device, the combination of LSM6DSL + LIS2MDL is much better option.

In terms of accuracy, current consumption, embedded features, and so on the combination of these two devices is much better.