Skip to main content
Associate III
Sep 11, 2024 12:43 PM UTC
Question

Actual Detection Range and FOV of STHS34PF80?

Hello everyone,

I’ve been working with the STHS34PF80 sensor and would appreciate some insights regarding its detection range and field of view (FOV). In my tests, I’ve observed that the sensor detects presence effectively up to a range of about 1 meter when I set the presence threshold to 100 LSB. Additionally, the FOV seems to be around 30 degrees.

I’m wondering if these results align with what others have experienced. Is this the typical range and FOV for this sensor under similar conditions, or could there be some optimization or calibration that I’m missing? Any feedback or suggestions would be greatly appreciated!

Thanks in advance!

 

Note

sensor config:

lpf_m: 04, lpf_p: 04, lpf_p_m: 02, lpf_a_t: 00

sths34pf80_gain_mode_get 7
sths34pf80_tobject_sensitivity_get 2000
sths34pf80_odr_get 8
sths34pf80_block_data_update_get 1
sths34pf80_one_shot_get 0
sths34pf80_presence_abs_value_get 1
sths34pf80_tobject_algo_compensation_get 1
sths34pf80_presence_hysteresis_get 25
sths34pf80_motion_hysteresis_get 25
sths34pf80_tambient_shock_threshold_get 10
sths34pf80_motion_threshold_get 100
sths34pf80_presence_threshold_get 150

 

This topic has been closed for replies.

3 replies

Federica Bossi
ST Technical Moderator
Sep 20, 2024 9:59 AM UTC

Hi @mobaid ,

We see no problem in the used configuration.

The expected FOV and detection range are much larger.

Can you give us more information about the test environment and conditions?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
mobaidAuthor
Associate III
Sep 22, 2024 2:05 PM UTC

Hi @Federica Bossi ,
Here are the test environment conditions :

 

T ambient

23’C ~ 25’C (Air conditioner)

Application

Indoor office

Sensor to Wall distance

3m

Sensor Hight

1m

Lens

N/A

AVG_TMOS : Number of averaged samples for object temperature

32

AVG_T : Number of averaged samples for ambient temperature

8

Interrupt source

Presence

Presence and motion detection setting

Presence threshold

150

Presence hysteresis

25

Motion threshold

100

Motion hysteresis

25

 

Thank you .