Skip to main content
Associate
December 12, 2023
Question

AcousticBF

Can the AcousticBF beamforming algorithm from FP-AUD-SMARTMIC1 algorithm be used on the entry-level kit of BlueCoin board (STEVAL-BCNCS01V1) to achieve audio acquisition at a sampling rate of 48kHz?

This topic has been closed for replies.

3 replies

Federica Bossi
ST Technical Moderator
December 12, 2023

Hi @insist_66 ,

Welcome to ST Community!

The library AcousticBF can't work at 48KHz 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
insist_66Author
Associate
December 12, 2023

The audio signal is obtained from the digital MEMSM Kefeng as a 1-bit PDM signal, which is then converted into a 16 bit PCM sample by a PDM to PCM conversion filter at 16 kHz. Using the AcousticBF algorithm in FP-AUD-SMARTMIC1, can a sampling rate of 48KHZ be achieved

Federica Bossi
ST Technical Moderator
December 13, 2023

Hi @insist_66 ,

I think there is a misunderstanding: the library only works up to 16KHz, both input and output.
We don't have libraries or examples that from a 16KHz input signal would allow a 48KHz output signal.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.