Skip to main content
JJońs.1
Associate
October 12, 2021
Solved

Accelerometers, 2g, low noise < 100 μg, I2C with SA0 and SA1 to connect 4 devices

I am looking for accelerometer ultra low noise with low g.

I want to connect 4 sensors using I2C, so I need 2 pin SA0 and SA1.

Do you have such sensors

This topic has been closed for replies.
JWu.12
JWu.12Best answer
Visitor II
October 14, 2021

Hi, from my experience there isn't, if you want to connect multiple devices you need to use the SPI lines.

Otherwise, if you don't need to acquire signals simultaneously, you can use one of the accelerometers (for example the LIS2DW12) and read first from two of them, keeping the CS of the other two high and writing the I2C_DISABLE bit of the CTRL2 (21h) register to 1, in order to disable the I2C block. But I guess this is not the best solution ever.

https://www.st.com/resource/en/datasheet/lis2dw12.pdf

3 replies

JWu.12
JWu.12Best answer
Visitor II
October 14, 2021

Hi, from my experience there isn't, if you want to connect multiple devices you need to use the SPI lines.

Otherwise, if you don't need to acquire signals simultaneously, you can use one of the accelerometers (for example the LIS2DW12) and read first from two of them, keeping the CS of the other two high and writing the I2C_DISABLE bit of the CTRL2 (21h) register to 1, in order to disable the I2C block. But I guess this is not the best solution ever.

https://www.st.com/resource/en/datasheet/lis2dw12.pdf

JJońs.1
JJońs.1Author
Associate
October 14, 2021
OK, thank you for your answer.
I have one more question. So far I used accelerometer NXP FXLS8471Q (end of life) 14 bits. Do you have accelerometer LLGA16 (3x3x1mm) which is 14 or 16 bits. LIS331DLH and LIS3DH looks good, the same footprint but only 12 bits

Regards,
Janusz Jonski
JWu.12
Visitor II
October 15, 2021

Hi Janusz, for effective 14 or 16 bit resolution I believe you have to change package into the LIS2DW12, for example.

There was the LIS3DSH satisfying your requirements, but I believe it is nrnd now.