Skip to main content
Ankur Shanker
Associate II
May 5, 2018
Question

Accelerometer selection for vibration analysis

Posted on May 05, 2018 at 08:01

Hello, we are building an application for condition monitoring of machines. For this, I am trying to figure out the appropriate accelerometer with the following specs: (1) a frequency response of 1.5 to 2 kHz, (2) a high ODR, higher the better, (3) an analog anti-aliasing filter, and (4) a resolution of at least 14 bits. After looking at different accelerometers, I have zeroed-in on LSM303AH and ISM330DLC (we'll be utilizing only the acc sensor). Can you please suggest which among the two should be preferred over the other (for this particular application)? Or, if these are not the appropriate ones, could you please suggest other options.

Regards,

Ankur

#accelerometer #vibration
This topic has been closed for replies.

6 replies

ST Employee
May 6, 2018
Posted on May 06, 2018 at 14:22

I would suggest to use ISM330DLC because it has 4kB and works from 1.71V to 3.6V.

The LSM303AH has only 256-lvele FIFO and works only at 1.8V.

Ankur Shanker
Associate II
May 7, 2018
Posted on May 07, 2018 at 16:48

Thanks Miroslav for your suggestion. Is it also possible for you to find

out what kind of anti-aliasing filter is implemented in ISM330DLC?

Best regards,

Ankur

On Sun, May 6, 2018 at 5:53 PM, Miroslav B <st-microelectronics@jiveon.com>

ST Employee
May 9, 2018
Posted on May 09, 2018 at 08:31

Unfortunately, this kid of information cannot be shared on the forum.