Skip to main content
Associate III
Feb 3, 2026 8:37 AM UTC
Solved

Accelerometer data acquisition timing vs microcontroller read timing

The microcontroller acquires data via SPI communication with the accelerometer. What is the risk if the data update timing of the accelerometer and the data acquisition timing of the microcontroller overlap?

ggobBest answer
Associate III
Feb 4, 2026 2:03 AM UTC

You mentioned in the following topic

Solved: ASM330LHH Frequency Measurement using the mother U... - STMicroelectronics Community

“keep in mind that it will be asynchronous, so you could loose some data” would that be “an inconsistent sample”?

 

6 replies

Federica Bossi
ST Technical Moderator
Feb 3, 2026 10:27 AM UTC

Hi @ggob ,

If the accelerometer updates its output registers at the same time the microcontroller is reading them over SPI, the main risk is that you get an inconsistent sample, not physical damage.

To mitigate this effect you could:

  1. Enable BDU in the accelerometer configuration.
  2. Use the data‑ready interrupt/flag to trigger the SPI read.
  3. Always read all the data registers belonging to one sample in a single burst transfer.
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ggobAuthorBest answer
Associate III
Feb 4, 2026 2:03 AM UTC

You mentioned in the following topic

Solved: ASM330LHH Frequency Measurement using the mother U... - STMicroelectronics Community

“keep in mind that it will be asynchronous, so you could loose some data” would that be “an inconsistent sample”?

 

Associate III
Feb 3, 2026 11:00 AM UTC

The risk is corrupted data, which will result in 0 data or some random numbers. An example would be unprotected memory pools, which are accessed by the MCU and the DMA.

 

What would I do in your position?

 

Build your system with a double buffered DMA with a timer as trigger to fetch the data. Use the callbacks to have an interrupt, when the buffer is half full, zero copy the data into a regular buffer in RAM and then proceed. You will need proper MPU or dedicated cache maintainance, depending on your MCU.

As reward you get a system with minimal overhead, reliable data stream and maximum performance.

ggobAuthor
Associate III
Feb 4, 2026 2:09 AM UTC

Thank you very much. It will be very useful.

TDK
Feb 3, 2026 2:11 PM UTC

You need to be more specific. What accelerometer? What does the datasheet say about it?

Chips often have protections against reading out mismatched data.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ggobAuthor
Associate III
Feb 4, 2026 1:49 AM UTC

My apologies. I omitted an important detail.
The device is the ASM330LHH.

When starting a timer on the microcontroller and using that timer to read data from the ASM330LHH via SPI, I want to understand the situation that could occur if the ASM330LHH's sample data update timing coincides with the microcontroller's SPI communication data read timing.