Skip to main content
Mars Chen
Visitor II
April 30, 2018
Question

About VL53L0x

Posted on April 30, 2018 at 09:30

Hi All,

In my project, It has a cover above VL53L0x( about 5 cm). I want to know what kind of material that the VL53L0x will not to be disturbed by it.

It means VL53L0x can work well when a cover above it.

Thanks a lot.

Mars.

#vl53l0x #proximity-sensor
This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
May 7, 2018
Posted on May 08, 2018 at 00:58

Mars -

The coverglass can be made out of anything that is clear at 940nm and flat. So Acrylic or PMMA are the cheap things. Regular glass is good. As is Gorilla glass or Sapphires glass.The best thing you can do is put the sensor as close to the glass as possible. The trick is to prevent photons from hitting the glass and bouncing back into the sensor.

See the bug:

https://community.st.com/0D50X00009XkYs4SAF

. It has some good words.

There is also a video -

https://community.st.com/external-link.jspa?url=https%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3DBHM2CZVXZGc

It describes the issue and an ultimate solution. It references a different chip, butthe concept is the same.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.