Skip to main content
Associate III
Sep 26, 2025 5:32 AM UTC
Solved

About Embedded compensation for ASM330LHH

Regarding the statement in the ASM330LHH datasheet “Embedded compensation for high stability over temperature”, does this mean that each output is temperature compensated? Does the compensation value correspond to the memory contents loaded when the BOOT bit is set? What output behavior is expected if this read/boot operation fails?

 

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Oct 1, 2025 8:49 AM UTC

Hi @ggob ,

 

The statement “Embedded compensation for high stability over temperature” in the datasheet means that the sensor applies internal temperature compensation algorithms to each sensor output (accelerometer and gyroscope) to reduce drift and variation caused by temperature changes.

When the BOOT bit is set, the device reloads factory calibration and compensation parameters. These parameters include temperature compensation coefficients.

Failure to load these parameters results in degraded sensor performance with more temperature-induced errors.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Oct 1, 2025 8:49 AM UTC

Hi @ggob ,

 

The statement “Embedded compensation for high stability over temperature” in the datasheet means that the sensor applies internal temperature compensation algorithms to each sensor output (accelerometer and gyroscope) to reduce drift and variation caused by temperature changes.

When the BOOT bit is set, the device reloads factory calibration and compensation parameters. These parameters include temperature compensation coefficients.

Failure to load these parameters results in degraded sensor performance with more temperature-induced errors.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ggobAuthor
Associate III
Oct 2, 2025 2:04 AM UTC

Thank you for your answer. It is very helpful.
If such a failure occurs, is there any way to detect it or to know that it has happened?