About accelerometer LIS3DH
- 1 reply
- 1088 views
I am considering an accelerometer.
The accelerometer is experimenting with LIS3DH.
I want to mount an acceleration sensor on a surgical light and
detect the movement of the lighting part of the surgical light.
I want to issue an INT interrupt when the light section is moved.
The light section hangs from the arm as shown in the photo linked below.
The movement is relatively slow and smooth.
https://www.skylux.co.jp/product/ixm_cj/
Currently, I am using Raspberry Pi 4 and conducting a motion detection
experiment with the LIS3DH evaluation program.
I'm in trouble because I can't detect slow movements.
When the X, Y, Z values were monitored,
the slow horizontal movement (about 7.5 cm / sec) was as shown in the attachment,
the value is buried in noise and the change cannot be detected.
Is it difficult with LIS3DH to detect relatively slow movements?
In addition, I would like to consider IIS2ICLX, IIS3DHHC, and IIS2DLPC,
which have relatively low noise levels.
Is it difficult to move slowly?
I would appreciate it if you could give me some advice.
Thank you.
Best Regards