Skip to main content
Associate
Jul 15, 2026 3:57 PM UTC
Solved

9 axis only gyroscope mems sensor available?

9 axis gyroscope mems sensor available?

Andrew Neil
Andrew NeilBest answer
Super User
Jul 16, 2026 9:29 AM UTC

Well, that’s the range of sensors which ST has.

If you don’t see anything there suitable for your (unstated) application requirements, then you’ll obviously have to look elsewhere.

 

But, as ​@TDK said, we live in a 3D world - so any real gyro can only have 3 axes

 

PS:

You can combine an LSM6DSOX + LIS3MDL to give you 9 DOF; eg,

https://www.adafruit.com/product/4517

 

Other sensors, of course, can be used: Basics of 6DOF and 9DOF sensor fusion

 

PPS:

See also:

which refers to:

Design tip DT0058, Computing tilt measurement and tilt-compensated eCompass

Design tip DT0060, Exploiting the gyroscope to update tilt measurement and eCompass

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

5 replies

Andrew Neil
Super User
Jul 15, 2026 4:15 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
Jul 15, 2026 10:02 PM UTC

It's 3 axis gyroscope u have send , i wanna know if 6 or 9 axis gyroscope mems exit for phones 

TDK
Jul 15, 2026 10:09 PM UTC

As the space we mortals inhabit is three dimensional, you will only see up to 3-axis gyroscopes here on Earth. Perhaps you are confusing this with a 9-DOF sensor.

"If you feel a post has answered your question, please click ""Accept as Solution""."